Less susceptible to interference, Bluetooth wireless technology offers a short-range wireless system which allows for highly confidential communications. As the application of this product expands to various areas such as automotive, home or office use, easy wireless connection will be available anytime and anywhere.

The Bluetooth brand and logo are owned by the Bluetooth SIG, Inc. and any use of such marks by Renesas is under license.

Lineup:

Embedded Solution

A solution which integrates Bluetooth communication functions (software+hardware) into Bluetooth chip sets while minimizing changes to the existing system.


SH7660

HCI Solution

A solution to develop a Bluetooth host which incorporates Renesas’ microprocessors. Bluetooth modules which use a Host Controller Interface(HCI) are introduced.


Evaluation Board

Evaluation Boards for the development of in-vehicle devices such as car navigation systems and car audio systems using the Bluetooth wireless technology.


Partner

Partner vendors for middleware that is used in the development of devices which support Bluetooth wireless technology.