Home /

New CPU 


 
Provide feedback
Print this page



New CPU
CPU Core Announcement
Compatibility with existing Renesas products
Concept of New CPU RX Family
Development of the RX family
RX family product lineup
System development environment for RX MCUs
The high-performance RX CPU architecture


News Release    20 May 2008


News Release    21 May 2007


News Release    8 Nov 2007


Presentation



On May 20, 2008, Renesas unveiled the high-speed, high-efficiency 32-bit MCU "RX600 series" for the new built-in CPU RX family.

New CPU RX Family

Announced in November 2007, the RX CPU architecture was developed as a new-generation CPU that achieves the high performance, low power consumption, greater code efficiency and greater cost performance called for in mid-range MCUs. The RX series powered by RX CPUs - the RX600 - features enhancements in performance and peripheral functions required by different applications and controlled objects.



The High-Speed, High-Efficiency "RX600 Series"

The 32-bit "RX600" MCU series with RX CPU is the high-speed, high-efficiency model of the RX family. The maximum operating frequency is 200 MHz, and the CPU features a 32-bit multiplier and 32-bit MAC (multiply and accumulate). In addition, the built-in floating-point unit enhances superior control operations such as digital filter and Fourier conversions. The lineup of general-purpose products and ASSP products is expanding for the RX600 as a 32-bit MCU series.
As the inaugural product in the lineup, Renesas plans to commercialize a general-purpose MCU with large-capacity memory for office automation equipment and consumer electronics. The engineering sample (ES) of the inaugural product is scheduled for release in the second quarter of 2009 (between April and June).
There are also plans to develop and expand a "RX200 series" focusing on low power consumption.

Outline of specifications for the RX600 series

CPURX CPU core
Maximum operating frequency200MHz
Power supply voltage3.0V / 3.3V / 5.0V
General-purpose register32-bit x 16
Floating-point unitSingle-precision floating-point unit (supporting add, substract compare, multiply, divide, etc.)
Memory protection unitYes (option)
DSP calculation functionYes (option)
Multiplier unit32-bit
Divider unitYes
Flash ROM (program)256KB-4MB
Flash ROM (Data)Yes
RAM64KB-256KB
Built-in peripheral functionsTimer
Serial interface
A/D converter
D/A converter
On-chip debuggingYes
Performance (target)1.25MIPS/MHz

Development by the MCU Development Platform

The RX family products are developed by the MCU development platform. Development through the platform makes it possible to provide products with a short TAT, and the products support customers who are working with rapidly-evolving systems. In addition, by structuring the peripheral functions of Renesas' existing MCUs - the H8S, H8SX, M16C and R32C series and so on - into IPs and turning them into assets, Renesas is able to pass on their functions to the RX family, while at the same time incorporating new functions without difficulty.

Even the Development Environment Can Be Shared with Existing Products

Compatibility of the development environment of the RX family is ensured with existing products by supporting the compiler language specifications and both big and little endians of the H8S, H8SX, M16C and R32C series, and providing the conversion tool from the assembler program.