|
Currently, the movement towards lead-free regulation to protect the
environment is spreading worldwide. Renesas Technology Corp. has been swiftly
working on the switchover to lead-free products to respond to this movement.
Fortunately, we can meet all the needs of lead-free products at the moment.
(*1)
Renesas lead-free products are thus compliant with the European RoHS Directive.
In addition, they have enough heat-resistance to enable mounting using an
Sn-Ag-Cu solder or similar lead-free solder with high melting point. (*2)
|