|
Documentation for H8S/H8SX LCD Direct Drive Technology Direct Drive LCD Design Guide (v2.6) Describes how to configure the Direct Drive LCD drivers to match the TFT-LCD panel manufacturer’s timing specifications, and describes the driver API. Also has an overview of system hardware and design recommendations. Direct Drive LCD Demonstration Application Note (v2.02) Describes in detail the program and source structure of the demonstration application.
Graphic API User’s Manual (v1.21) User’s guide for GAPI, a library of routines to allow for the simple creation and manipulation of raster based images in RAM memory frames.
Direct Drive LCD Presentation (Dec 2009) Presentation overview of TFT-LCD basics, Direct Drive LCD functionality and timing, application and tool information. This is a locked file. Click "Read Only" when asked for a password.
H8S/2426 "Z" Version Hardware Manual
H8S/2456 "Z" Version Hardware Manual
H8SX/1668M "Z" Version Hardware Manual
H8S/1665M "Z" Version Hardware Manual
Direct Drive TFT Panel List (March 2010) List of TFT-LCD panels from various manufacturers that have been driven by DDLCD method.
|