|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Renesas Electronics is a recognized pioneer in the development of USB silicon devices that successfully pass the USB Compliance Program. Its devices have been adopted in a large number of USB products already on the market. Renesas supplies a rich lineup of MCUs, ranging from small-package devices for Low-Speed USB application to Full-Speed MCUs, Hi-Speed MCUs, Hub MCUs, ASSPs using our own IP, System LSI and High-Speed devices, addressing the diversified needs of our customers and supporting all different types of products. Features:
With so many Renesas USB devices, it can be difficult to know which device to select. Click here for our quick selector guide on Renesas MCUs to find the device ideal for your application.
(click above to select) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Key Points: Flexible powering scehemes, low power, easy-to-use demos and software drivers, cost-sensitive applications and high performance coupled with full system connectivity make Renesas H8 MCU’s an ideal solution for USB connectibity system requirements. Renesas USB peripherals are fully USB v2.0 certified.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
The H8S and the H8SX product line offer USB connectivity with other application interfaces. Highlighted below are the main interface areas supported within the H8S and H8SX product line. The USB devices are all USB peripheral, USB v2.0 compliant running up to 12Mbps.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
All system connectivity (Ethernet, USB and TFT-LCD) is fully supported with third-party RTOS vendors. Click here for the list of RTOS vendors supporting the H8S and H8SX devices.
Because many of the USB devices will be used in mobile devices or power sensitive applications,the H8S and H8SX product line focus on lowest power implementations for USB applications. Below is a listing of how H8S and H8SX devices meet all low power requirements.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Multiple clock sources can be used for the MCU devices. These are for the system clock and USB clock. The USB peripheral has a dedicated PLL for the USB protocol implementation. This allows different crystals to be selected for lower power operation. The main system and perpherial clocks can be switched to the 32-kHz sub-clock for very low power operation. Or just the the 32-kHz RTC timer can run off the 32kHz sub clock for RTC operation. The clock to selected peripherals can be stopped (including the CPU). Therefore it is possible to run just the USB peripheral of its own clock source, as well as running the RTC off the 32-kHz sub clock with the rest of the system stopped, giving very low power operation. The H8S and H8SX have 5 power-down modes:
The standby modes are for low power. For example software standby mode consumes just 3uA (typical) and the system can be woken up from an external interrupt. As the CPU core is completely static, the CPU will wake up quickly from the external interrupt and execute from the PC register location. Bus Powered or Self Powered USB applications, for example portable devices running off a battery, are usually very power sensitive. Anyway to reduce power consumption is important for USB connectivity. As well as the power down modes listed above Renesas H8 USB MCU devices offer flexibility in the USB powering. Easy-to-Use Demos, Software Drivers
Performance, low power and products is only half the issue with USB connectivity. Most important is ease of use. This is the main area of focus within Renesas USB MCUs.
In order to offer full support and ease of use the following are available:
HID (Human Interface Device) drivers: Human Interface Devices are used in nearly every modern computer. Examples are include keyboards, mice and game controllers. This interface uses the control and interrupt communication pipes. MSC (Mass Storage Device Class) drivers: MSC is the common acronym for devices supporting this type of interface. UMS (Universal Mass Storage) has become common as online jargon. This interface offers a simple interface to read and write sectors of data. This interface uses the control and bulk communication pipes. COMMs (Serial to USB): A driver to convert USB to a PC serial communication interface. Bulk (USB bulk transfer example): A user example of maximum data transfer rate.
Renesas offers different developers kits for various application requirements. Below are listed the developer kits and an overview of what they contain:
H8S/2218 ? Low Power USB for High performance, low power cost sensitive applications
H8SX/1664 ? High performance, System Connectivity
Documentation and Application Notes H8S2218
H8SX/1664
H8S/2215R
Cost sensitive applications and high performance Now that you realize how Renesas MCUs can meet your system requirements, the remaining issue is to find the exact MCU device which is right for you. The table giving basic partition of Renesas USB devices |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Lineup:
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||