Issue Date: 17 December 2009

 

Note:

  • IO Wizard is free and unsupported utility. We do not make any commitment to update this software in the event of bugs being found, nor do we make any commitment to inform the user of any changes. By downloading this software the user is assuming responsibility for its use and the decision to incorporate any code generated by the utility in any application. The source code for this software is not available to users.
  • IO Wizard aids new Renesas microcomputer (MCU) users to make initialization setting in the source code.
  • User input the device selection, system setting and peripheral operation setting through GUI.
  • After all settings are done, user can proceed to run code generation.
  • The output files have to go through code compilation process before user can obtain the object file.
  • Error: InstallShield error code -6001 during setup

Solution:

This InstallShield errorindicates a corrupt verison of InstallShield is installed on your computer. To correct this issue, simply delete the following folder from your computer and attempt to run the installer again:
C:\Program Files\Common Files\InstallShield\Professional\RunTime\0701

If this fails to correct the problem, we recommend you RENAME (not delete) the entire C:\Program Files\Common Files\InstallShield\ folder and try again.

You may rename the folder to anything you like, but we recommend something similar to 'InstallShield-old'.

Download

Product Name File Name File Size Download Link
IO Wizard Peripheral Code Generator IO_Wizardv132r01.exe 8.50 MB